AXIS#.LOAD.INERTIA

Description

AXIS#.LOAD.INERTIA sets the load inertia.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

kgcm² for rotary motors

Range

1 to 1,000,000 kgcm² or kg

Default Value

0 kgcm² or kg

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.LOAD.INERTIA

5014h

01h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.LOAD.INERTIA

5114h

01h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5700

1

5700 (0x1644)

AXIS1.LOAD.INERTIA

Unsigned32

Read/Write

Yes

71236

2

5700 (0x1644)

AXIS2.LOAD.INERTIA

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.LOAD.INERTIA

5700

Float

Read/Write

-